Feedback_Limit_Speed

Index.Sub 2230.1BH
Data Type Unsigned16
Access Read/Write
PDO Mappable RX_PDO (1)
Unit

rpm

Range

0 to 4000
Default Value 3000
Store Supported Yes
Description This value is used for Closed Loop feature and defines the maximum motor speed.

Notes

(1) Available with firmware V03r07 or superior.